google play store access in lolipop prebuilt image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

google play store access in lolipop prebuilt image

750 Views
sachusanal
Contributor III

Dear Sir ,

I am using the Android lolipop prebuilt image for my imx6qsabrsd board.

I developed one apk for this . in that apk i need to do navigation .

the navigation property is working wit the google play store services. how can access google play store in my this build.

is it possible to install google play store in this build.

I try to download and install the  play store apk manuvally.

the apk is installed but it closed forcefully

please help me to solve this issue.

Labels (1)
0 Kudos
3 Replies

487 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

The Play store is part of a pack of applications provided by Google by separate, called Google Apps (or gapps). If you want to add them to your Android device, you should contact directly to Google in order to get them.


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

487 Views
sachusanal
Contributor III

in my board i am using prebuilt lolipop android image which is provided from freescale. I download google playstore from the net and insatlled but it forcefully closed what is the reason for that

0 Kudos

487 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

It could be a good idea if you post such question on Google support and/or forums, as this is not part of the Freescale Release BSP.

Hope this will be useful for you.

Best regards!

/Carlos

0 Kudos