Dear freescale,
目前我们的imx6dl的车载导航项目已经在android4.4上开发完毕,因freescale发布的android5.0的 BSP,想将我们的系统升级到android5.0,我们使用的是美光的EMMC MTFC8GACAAAM-4M IT
,EMMC使用的是SD4接口,跟imx6dl开发板是一致,只是使用的型号不一样,并且PMIC芯片也跟开发板一致,内存是1G,我看了uboot的CFG文件也跟开发板一致的。我的想法是先不管其它外设部分,先保证能够下载并且uboot跑起来,之后在考虑移植其它外设部分。因为之前使用的内核时3.0.35版本的,现在android5.0使用的是3.10.53,使用的是dts的方式配置,所以要修改内核的话,还要学习学习。
其中CFG.ini配置:
[profiles]
chip = Linux
[platform]
board = SabreSD
[LIST]
name = SDCard
[variable]
board = sabresd
mmc = 2
sxuboot=17x17arm2
sxdtb=17x17-arm2
ldo=
UICFG.ini内容:
[UICfg]
PortMgrDlg=1
mfgtool2-android-mx6dl-sabresd-emmc.vbs文件中将mmc=3 修改成2,之后点击运行mfgtool2-android-mx6dl-sabresd-emmc.vbs。下载的时候提示如附件。
发现运行到:
UTP: sending Success to kernel for command $ echo 8 > /sys/block/mmcblk3/device/boot_config.
utp_poll: pass returned.
UTP: received command '$ ls -l /dev/mmc* '
UTP: executing "ls -l /dev/mmc* "
之后就不再运行了,关于android5.0的下载移植,freescale有没什么好的文档嘛,我应该怎么修改系统和MFGTool工具才能正常下载 ???
怎么给我的感觉imx6q和imx6dl发布的BSP是针对SD卡的,而不是EMMC的一样????
谢谢!
Original Attachment has been moved to: android.5.0_downloader---4.log.zip
Dear freescale,
不修改android_L5.0.0_1.0.0-ga_tools工具的任何文件,只将编译freescale网站上下载的imx6 android5.0 的BSP包,将编译后生成的文件拷贝到mfgtools\mfgtools\Profiles\Linux\OS Firmware\files\android\sabresd目录下,之后直接点击mfgtools/mfgtool2-android-mx6dl-sabresd-emmc.vbs运行,
发现工具运行到ucl2.xml文件的
<CMD state="Updater" type="push" body="$ mkfs.ext4 -b 4096 -m 0 -O ^flex_bg,^uninit_bg /dev/mmcblk%mmc%p4">Formatting data partition</CMD>
这个语句就一直停在那里了,没往下运行。而mfgtool工具显示:
log如下:
U-Boot 2014.04 (Jan 05 2015 - 14:56:32)
CPU: Freescale i.MX6DL rev1.2 at 792 MHz
CPU: Temperature 42 C, calibration data: 0x5964e37d
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
MMC: no card present
MMC init failed
Using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Found PFUZE100 deviceid=10,revid=21
MMC: no card present
mmc1(part 0) is current device
Net: Phy not found
PHY reset timed out
FEC [PRIME]
Warning: failed to set MAC address
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Kernel image @ 0x12000000 [ 0x000000 - 0x5093f0 ]
## Loading init Ramdisk from Legacy Image at 12c00000 ...
Image Name: fsl-image-mfgtool-initramfs-imx6
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 7338461 Bytes = 7 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Using Device Tree in place at 18000000, end 1800f3cb
switch to ldo_bypass mode!
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 3.10.53-1.1.0_ga-mfgtool+g496fbe0 (jenkins@scmbl1) (gcc version 4.8.2 (GCC) ) #1 SMP Mon Jan 5 14:49:15 CST 2015
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 DualLite SABRE Smart Device Board(PFUZE100)
cma: CMA: reserved 320 MiB at 3c000000
Memory policy: ECC disabled, Data cache writealloc
PERCPU: Embedded 8 pages/cpu @81528000 s8768 r8192 d15808 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= enable_wait_mode=off
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1024MB = 1024MB total
Memory: 690500k/690500k available, 358076k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xc0800000 - 0xff000000 (1000 MB)
lowmem : 0x80000000 - 0xc0000000 (1024 MB)
modules : 0x7f000000 - 0x80000000 ( 16 MB)
.text : 0x80008000 - 0x80c0862c (12290 kB)
.init : 0x80c09000 - 0x80c5b240 ( 329 kB)
.data : 0x80c5c000 - 0x80cad180 ( 325 kB)
.bss : 0x80cad180 - 0x80d0f714 ( 394 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
Hierarchical RCU implementation.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32050000, Cache size: 524288 B
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
CPU identified as i.MX6DL, silicon rev 1.2
Console: colour dummy device 80x30
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x80639f00 - 0x80639f58
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
Brought up 2 CPUs
SMP: Total of 2 processors activated (3162.11 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
pinctrl core: initialized pinctrl subsystem
regulator-dummy: no parameters
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
Use WDOG2 as reset source
syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
vdd1p1: 800 <--> 1375 mV at 1125 mV
vdd3p0: 2800 <--> 3150 mV at 3000 mV
vdd2p5: 2000 <--> 2750 mV at 2425 mV
cpu: 725 <--> 1450 mV
vddpu: 725 <--> 1450 mV
vddsoc: 725 <--> 1450 mV
syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6dl-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
bio: create slab <bio-0> at 0
mxs-dma 110000.dma-apbh: initialized
usb_otg_vbus: 5000 mV
usb_h1_vbus: 5000 mV
wm8962-supply: no parameters
mipi_dsi_pwr_on: no parameters
sensor-supply: 3300 mV
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-1: IMX I2C adapter registered
i2c i2c-2: Max17135 PMIC not found!
i2c i2c-2: IMX I2C adapter registered
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
cfg80211: Calling CRDA to update world regulatory domain
pureg-dummy: no parameters
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP: reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 7160K (82c01000 - 832ff000)
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
Bus freq driver module loaded
futex hash table entries: 512 (order: 3, 32768 bytes)
VFS: Disk quotas dquot_6.5.2
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.22)
msgmni has been set to 2002
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: WEIM driver registered.
mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
mxc_sdc_fb fb.31: registered mxc display driver ldb
imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 128x48
mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0x1a:0xa0:0xc1
fbcvt: 1920x1080@60: CVT Name - 2.073M9
mxc_sdc_fb fb.32: registered mxc display driver hdmi
imx_epdc_fb 20f4000.epdc: Unable to get display PMIC regulator.err = 0xfffffdfb
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: loaded firmware 1.1
imx-sdma 20ec000.sdma: initialized
pfuze100-regulator 1-0008: Full lay: 2, Metal lay: 1
pfuze100-regulator 1-0008: FAB: 0, FIN: 0
pfuze100-regulator 1-0008: pfuze100 found.
SW1AB: 300 <--> 1875 mV at 1175 mV
SW1C: 300 <--> 1875 mV at 1175 mV
SW2: 800 <--> 3300 mV at 3300 mV
SW3A: 400 <--> 1975 mV at 1500 mV
SW3B: 400 <--> 1975 mV at 1500 mV
SW4: 800 <--> 3300 mV at 3150 mV
SWBST: 5000 <--> 5150 mV at 5000 mV
VSNVS: 1000 <--> 3000 mV at 3000 mV
VREFDDR: 750 mV
VGEN1: 800 <--> 1550 mV at 1500 mV
VGEN2: 800 <--> 1550 mV at 1500 mV
VGEN3: 1800 <--> 3300 mV at 2800 mV
VGEN4: 1800 <--> 3300 mV at 1800 mV
VGEN5: 1800 <--> 3300 mV at 3000 mV
VGEN6: 1800 <--> 3300 mV at 3300 mV
Serial: IMX driver
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled
serial: Freescale lpuart driver
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
of_dma_request_slave_channel: dma-names property missing or empty
spi_imx 2008000.ecspi: cannot get the TX DMA channel!
spi_imx 2008000.ecspi: dma setup error,use pio instead
m25p80 spi32766.0: found mr25h256, expected m25p32
m25p80 spi32766.0: mr25h256 (32 Kbytes)
spi_imx 2008000.ecspi: probed
fec 2188000.ethernet (unregistered net_device): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unregistered net_device): Using random MAC address: ae:2f:a5:f7:e9:01
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
usbcore: registered new interface driver usb-storage
ci_hdrc ci_hdrc.1: doesn't support gadget
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
elan-touch 2-0010: elan - Read Hello Packet Failed
elan-touch: probe of 2-0010 failed with error -5
egalax_ts 1-0004: Failed to read firmware version
egalax_ts: probe of 1-0004 failed with error -5
egalax_ts 2-0004: Failed to read firmware version
egalax_ts: probe of 2-0004 failed with error -5
input: max11801_ts as /devices/soc0/soc.1/2100000.aips-bus/21a4000.i2c/i2c-1/1-0048/input/input0
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
mxc_v4l2_output v4l2_out.37: V4L2 device registered as video16
mxc_v4l2_output v4l2_out.37: V4L2 device registered as video17
mxc_v4l2_output v4l2_out.37: V4L2 device registered as video18
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
mag3110 2-000e: check mag3110 chip ID
mag3110 2-000e: read chip ID 0xfffffffb is not equal to 0xc4!
mag3110: probe of 2-000e failed with error -22
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
mma8451 0-001c: read chip ID 0x1 is not equal to 0x1a or 0x2a!
mma8451: probe of 0-001c failed with error -22
imx2-wdt 20c0000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
cpuidle: using governor ladder
cpuidle: using governor menu
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc1: no vqmmc regulator found
mmc1: no vmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
mmc2: no vqmmc regulator found
mmc2: no vmmc regulator found
mmc1: new high speed SDIO card at address 0001
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mmc3: no vqmmc regulator found
mmc3: no vmmc regulator found
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
galcore: clk_get vg clock failed, disable vg!
Galcore version 5.0.11.25762
mmc3: BKOPS_EN bit is not set
mmc3: new high speed DDR MMC card at address 0001
mmcblk3: mmc3:0001 P1XXXX 7.20 GiB
mmcblk3boot0: mmc3:0001 P1XXXX partition 1 16.0 MiB
mmcblk3boot1: mmc3:0001 P1XXXX partition 2 16.0 MiB
mmcblk3rpmb: mmc3:0001 P1XXXX partition 3 128 KiB
mmcblk3: p1 p2 p3 < p5 p6 p7 > p4
mmcblk3: p4 size 12926976 extends beyond EOD, truncated
mmcblk3boot1: unknown partition table
mmcblk3boot0: unknown partition table
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_asrc 2034000.asrc: mxc_asrc registered
mxc_vpu 2040000.vpu: VPU initialized
caam 2100000.caam: Instantiated RNG4 SH0
caam 2100000.caam: Instantiated RNG4 SH1
caam 2100000.caam: device ID = 0x0a160100 (Era 4)
caam 2100000.caam: job rings = 2, qi = 0
caam algorithms registered in /proc/crypto
caam_jr 2101000.jr0: registering rng-caam
platform caam_sm: blkkey_ex: 4 keystore units available
platform caam_sm: 64-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: 64-bit black key:
platform caam_sm: [0000] a1 29 4b f2 0b 06 6e d9
platform caam_sm: [0008] 05 e3 15 d3 9c de 05 b1
platform caam_sm: 128-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: 128-bit black key:
platform caam_sm: [0000] 8d a8 40 2f 92 1f 5f a2
platform caam_sm: [0008] 3a 68 72 93 82 f9 a3 de
platform caam_sm: 192-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: 192-bit black key:
platform caam_sm: [0000] 17 09 7f eb 3e 27 05 63
platform caam_sm: [0008] 10 ec 62 c4 da 84 ce 74
platform caam_sm: [0016] 0a 8c 09 20 48 94 e5 82
platform caam_sm: [0024] 6f c2 39 b0 63 29 3e b4
platform caam_sm: 256-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
platform caam_sm: 256-bit black key:
platform caam_sm: [0000] 77 3c df a7 47 69 ff dc
platform caam_sm: [0008] cf 0d 44 2c e7 52 44 e7
platform caam_sm: [0016] e6 b9 5d ce 95 2c 17 b1
platform caam_sm: [0024] 91 b0 e4 5b 39 a2 dd fa
platform caam_sm: 64-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 196-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 64-bit black key in blob:
platform caam_sm: [0000] 4b d3 4e 2c 6c 5a c4 04
platform caam_sm: [0008] ac 66 8c 5a 5d 01 dd b8
platform caam_sm: [0016] d6 45 f3 00 63 74 e6 a1
platform caam_sm: [0024] ba 15 d7 82 ba dd 31 c5
platform caam_sm: [0032] a1 db f8 c8 f1 ab 18 d5
platform caam_sm: [0040] 7d ed bb db 94 95 ec 9a
platform caam_sm: [0048] 27 85 c0 c2 7c 78 83 c3
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit black key in blob:
platform caam_sm: [0000] 89 ee 96 fc 5b cc 6b b7
platform caam_sm: [0008] 61 4e fb 6f 3b 8e d7 a2
platform caam_sm: [0016] 87 43 27 97 c4 42 7b 6d
platform caam_sm: [0024] c5 74 c1 62 87 02 9c 5a
platform caam_sm: [0032] 18 6c 67 d1 b3 5e fa b1
platform caam_sm: [0040] 99 59 fd af 2d c8 f4 83
platform caam_sm: [0048] 2f 50 41 8e 5c 29 d1 83
platform caam_sm: [0056] ce c6 85 38 70 8a 50 c1
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 192-bit black key in blob:
platform caam_sm: [0000] 2a 17 4a 9c c9 c4 4c bc
platform caam_sm: [0008] ef 73 dd ce bb 46 55 43
platform caam_sm: [0016] b0 06 71 34 d2 6a 69 ee
platform caam_sm: [0024] 48 31 94 ab 98 3c 38 77
platform caam_sm: [0032] 1e fd f2 37 2d f9 17 1c
platform caam_sm: [0040] 46 dc 23 c4 66 94 de 9c
platform caam_sm: [0048] bc 36 19 cc de d4 63 91
platform caam_sm: [0056] 68 fa ab f1 45 5d 27 b9
platform caam_sm: [0064] 2f ba c2 00 5f 64 23 32
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit black key in blob:
platform caam_sm: [0000] 0c aa 5c db 2e 2d a7 cf
platform caam_sm: [0008] 44 16 e0 aa ef c9 68 f3
platform caam_sm: [0016] 61 4c d1 57 69 83 15 5b
platform caam_sm: [0024] 95 84 6a 1b 92 94 36 c9
platform caam_sm: [0032] d0 c0 fc e7 74 11 74 1f
platform caam_sm: [0040] b9 a6 e6 e3 80 97 c2 7e
platform caam_sm: [0048] e0 25 f2 5b 60 62 1b bf
platform caam_sm: [0056] 0e 7b a7 1c 06 69 2f 8b
platform caam_sm: [0064] e4 e0 2d 27 aa f3 4e a9
platform caam_sm: [0072] 54 a5 5d c2 2c 24 f6 f0
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: restored 64-bit black key:
platform caam_sm: [0000] ee ba c4 93 0a 42 20 f2
platform caam_sm: [0008] e7 8e 2b 75 bb 00 7d 00
platform caam_sm: restored 128-bit black key:
platform caam_sm: [0000] 8d a8 40 2f 92 1f 5f a2
platform caam_sm: [0008] 3a 68 72 93 82 f9 a3 de
platform caam_sm: restored 192-bit black key:
platform caam_sm: [0000] 17 09 7f eb 3e 27 05 63
platform caam_sm: [0008] 10 ec 62 c4 da 84 ce 74
platform caam_sm: [0016] ac b5 1c 76 ec 9d 2a 48
platform caam_sm: [0024] 2c 50 da e3 ed ff d0 5e
platform caam_sm: restored 256-bit black key:
platform caam_sm: [0000] 77 3c df a7 47 69 ff dc
platform caam_sm: [0008] cf 0d 44 2c e7 52 44 e7
platform caam_sm: [0016] e6 b9 5d ce 95 2c 17 b1
platform caam_sm: [0024] 91 b0 e4 5b 39 a2 dd fa
snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
wm8962 0-001a: Failed to read ID register
wm8962: probe of 0-001a failed with error -5
imx-wm8962 sound.29: failed to find codec platform device
imx-wm8962: probe of sound.29 failed with error -22
imx-audio-hdmi sound-hdmi.30: hdmi-hifi <-> hdmi_audio.17 mapping ok
TCP: cubic registered
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
VGEN3: disabling
VGEN2: disabling
VGEN1: disabling
SWBST: disabling
SW4: disabling
wm8962-supply: disabling
usb_otg_vbus: disabling
regulator-dummy: disabling
imx mcc test is registered.
g_mass_storage gadget: Mass Storage Function, version: 2009/09/11
g_mass_storage gadget: Number of LUNs=1
lun0: LUN: removable file: (no medium)
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
input: gpio-keys.28 as /devices/soc0/gpio-keys.28/input/input1
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:02 UTC (2)
ALSA device list:
#0: imx-hdmi-soc
Freeing unused kernel memory: 328K (80c09000 - 80c5b000)
Starting UTP
uuc 0.5 [built Jan 16 2015 13:53:24]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
max8903-charger max8903.19: Charger suffers a fault and stops.
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ tar xf $FILE '
UTP: executing "tar xf $FILE "
UTP: sending Success to kernel for command $ tar xf $FILE .
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
utp_poll: pass returned.
UTP: received command '$ sh mksdcard-android.sh /dev/mmcblk3'
UTP: executing "sh mksdcard-android.sh /dev/mmcblk3"
1+0 records in
1+0 records out
1024 bytes (1.0 kB) copied, 0.455468 s, 2.2 kB/s
sfdisk: Checking that no-one is using th mmcblk3: unknown partition table
is disk right now ...
sfdisk: OK
Disk /dev/mmcblk3: 236032 cylinders, 4 heads, 16 sectors/track
sfdisk: /dev/mmcblk3: unrecognized partition tabl mmcblk3: p1 p2 p3 < p5 p6 p7 > p4
e type
Old situation:
sfdisk: Nmmcblk3: p4 size 12926976 extends beyond EOD, o partitions found
sfdisk: Warnitruncated
ng: given size (6312) exceeds max allowable size (6272)
New situation:
Units: 1MiB = 1024*1024 bytes, blocks of 1024 bytes, counting from 0
Device Boot Start End MiB #blocks I mmcblk3: p1 p2 p3 < p5 p6 p7 > p4
d System
/dev/mmcblk3p1 mmcblk3: p4 size 12926976 extends beyond EOD, 0+ 15 16- 16383+ 83 truncated
Linux
/dev/mmcblk3p2 16 23 8 8192 83 Linux
/dev/mmcblk3p3 24 1103 1080 1105920 5 Ex mmcblk3: p1 p2 p3 < p5 p6 p7 > p4
tended
/dev/mmcblk3p4 1104 mmcblk3: p4 size 12926976 extends beyond EOD, 7415 6312 6463488 83 Litruncated
nux
/dev/mmcblk3p5 24+ 535 512- 524287+ 83 Linux
/dev/mmcblk3p6 536+ 1047 512- 524287+ 83 Linux
/dev/mmcblk3p7 1048+ 1055 8- 8191+ 83 Linux
/dev/mmcblk3p8 1056+ 1061 6- 6143+ 83 Linux
/dev/mmcblk3p9 1062+ 1063 2- 2047+ 83 Linux
sfdisk: Warning: partition 4 extends past end of disk
Successfully wrote the new partition table
Re-reading the partition table ...
sfdisk: If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)
to zero the first 512 bytes: dd if=/dev/zero of=/dev/foo7 bs=512 count=1
(See fdisk(8).)
sfdisk: Checking that no-one is using this disk right now ...
sfdisk: OK
Disk /dev/mmcblk3: 236032 cylinders, 4 heads, 16 sectors/track
Old situation:
Units: 1MiB = 1024*1024 bytes, blocks of 1024 bytes, counting from 0
Device Boot Start End MiB #blocks Id System
/dev/mmcblk3p1 0+ 15 16- 16383+ 83 Linux
/dev/mmcblk3p2 16 23 8 8192 83 Linux
/dev/mmcblk3p3 24 1103 1080 1105920 5 Extended
/dev/mmutp_poll: pass returned.
cblk3p4 1104 7415 6312 6463488 83 Linux
/dev/mmcblk3p5 24+ 535 512- 524287+ 83 Linux
/dev/mmcblk3p6 536+ 1047 512- 524287+ 83 Linux
/dev/mmcblk3p7 1048+ 1055 8- 8191+ 83 Linux
/dev/mmcblk3p8 1056+ 1061 6- 6143+ 83 Linux
/dev/mmcblk3p9 1062+ 1063 2- 2047+ 83 Linux
New situation:
Units: 1MiB = 1024*1024 bytes, blocks of 1024 bytes, counting from 0
Device Boot Start End MiB #blocks Id System
/dev/mmcblk3p1 8 15 8 8192 83 Linux
/dev/mmcblk3p2 16 23 8 8192 83 Linux
/dev/mmcblk3p3 24 1103 1080 1105920 5 Extended
/dev/mmcblk3p4 1104 7415 6312 6463488 83 Linux
/dev/mmcblk3p5 24+ 535 512- 524287+ 83 Linux
/dev/mmcblk3p6 536+ 1047 512- 524287+ 83 Linux
/dev/mmcblk3p7 1048+ 1055 8- 8191+ 83 Linux
/dev/mmcblk3p8 1056+ 1061 6- 6143+ 83 Linux
/dev/mmcblk3p9 1062+ 1063 2- 2047+ 83 Linux
sfdisk: Warning: partition 4 extends past end of disk
Successfully wrote the new partition table
Re-reading the partition table ...
sfdisk: If you created or changed a DOS partition, /dev/foo7, say, then use dd(1)
to zero the first 512 bytes: dd if=/dev/zero of=/dev/foo7 bs=512 count=1
(See fdisk(8).)
UTP: sending Success to kernel for command $ sh mksdcard-android.sh /dev/mmcblk3.
UTP: received command '$ dd if=/dev/zero of=/dev/mmcblk3 bs=1k seek=384 conv=fsync count=129'
UTP: executing "dd if=/dev/zero of=/dev/mmcblk3 bs=1k seek=384 conv=fsync count=129"
129+0 records in
129+0 records out
132096 bytes (132 kB) copied, 0.0314607 s, 4.2 MB/s
UTP: sending Success to kernel for command $ dd if=/dev/zero of=/dev/mmcblk3 bs=1k seek=384 conv=fsync count=129.
utp_poll: pass returned.
UTP: received command '$ echo 0 > /sys/block/mmcblk3boot0/force_ro'
UTP: executing "echo 0 > /sys/block/mmcblk3boot0/force_ro"
UTP: sending Success to kernel for command $ echo 0 > /sys/block/mmcblk3boot0/force_ro.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ dd if=$FILE of=/dev/mmcblk3boot0 bs=512 seek=2'
UTP: executing "dd if=$FILE of=/dev/mmcblk3boot0 bs=512 seek=2"
766+0 records in
766+0 records out
392192 bytes (392 kB) copied, 0.212398 s, 1.8 MB/s
UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk3boot0 bs=512 seek=2.
utp_poll: pass returned.
UTP: received command '$ echo 1 > /sys/block/mmcblk3boot0/force_ro'
UTP: executing "echo 1 > /sys/block/mmcblk3boot0/force_ro"
UTP: sending Success to kernel for command $ echo 1 > /sys/block/mmcblk3boot0/force_ro.
utp_poll: pass returned.
UTP: received command '$ echo 8 > /sys/block/mmcblk3/device/boot_config'
UTP: executing "echo 8 > /sys/block/mmcblk3/device/boot_config"
UTP: sending Success to kernel for command $ echo 8 > /sys/block/mmcblk3/device/boot_config.
utp_poll: pass returned.
UTP: received command '$ ls -l /dev/mmc* '
UTP: executing "ls -l /dev/mmc* "
brw------- 1 root root 179, 0 Jan 1 00:00 /dev/mmcblk3
brw------- 1 root root 179, 8 Jan 1 00:00 /dev/mmcblk3boot0
brw------- 1 root root 179, 16 Jan 1 00:00 /dev/mmcblk3boot1
brw------- 1 root root 179, 1 Jan 1 00:00 /dev/mmcblk3p1
brw------- 1 root root 179, 2 Jan 1 00:00 /dev/mmcblk3p2
brw------- 1 root root 179, 3 Jan 1 00:00 /dev/mmcblk3p3
brw------- 1 root root 179, 4 Jan 1 00:00 /dev/mmcblk3p4
brw------- 1 root root 179, 5 Jan 1 00:00 /dev/mmcblk3p5
brw------- 1 root root 179, 6 Jan 1 00:00 /dev/mmcblk3p6
brw------- 1 root root 179, 7 Jan 1 00:00 /dev/mmcblk3p7
brw------- 1 root root 179, 24 Jan 1 00:00 /dev/mmcblk3rpmb
UTP: sending Success to kernel for command $ ls -l /dev/mmc* .
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ dd if=$FILE of=/dev/mmcblk3p1'
UTP: executing "dd if=$FILE of=/dev/mmcblk3p1"
14828+1 records in
14828+1 records out
7592192 bytes (7.6 MB) copied, 1.38154 s, 5.5 MB/s
UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk3p1.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext4 -b 4096 -m 0 -O ^flex_bg,^uninit_bg /dev/mmcblk3p4'
UTP: executing "mkfs.ext4 -b 4096 -m 0 -O ^flex_bg,^uninit_bg /dev/mmcblk3p4"
mke2fs 1.42.9 (28-Dec-2013)
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
Discarding device blocks: max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
max11801_ts 1-0048: FIFO_RD_AUX_MSB read fails
Hi zhaojingrong,
你这里是自己做的板子,我们官网提供的BSP是针对飞思卡尔的开发板的。你直接在你的板子上跑官网提供的BSP,在烧写或者启动过程中肯定会有问题的,这里建议你先做portting, 根据你自己设计的板子porting好BSP时,然后再编译在你的板子上跑才是OK的。
关于你帖中提到的另外一个问题,
关于android5.0的下载移植,freescale有没什么好的文档嘛,我应该怎么修改系统和MFGTool工具才能正常下载 ???
怎么给我的感觉imx6q和imx6dl发布的BSP是针对SD卡的,而不是EMMC的一样????
关于移植android5.0的文档我们这边没有,不过你可以参考linux BSP 的移植文档来操作,方法是差不多的。 还有SD和Emmc是差不多的,编译好的images你可以写到SD卡上也可以写到Emmc上,都是OK的,没有什么问题的。当然Emmc会比SD卡快一些的。
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
why you not say you do not konw?