AnsweredAssumed Answered

Mfgtools-Rel-4.1.0_130816_MX6Q_UPDATER not working...

Question asked by ioan Calapod on Aug 2, 2015
Latest reply on Aug 10, 2015 by igorpadykov

Hi All

 

I used the above tool to create a bootable SD for SABRE SD board (I.MX6 Quad)

Everything went smooth but when I tried to boot up into the SD card written I get this:

 

"U-Boot 2009.08 (Aug 16 2013 - 12:04:20)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz
Thermal sensor with ratio = 172
Temperature:   26 C, calibration data 0x5404987d
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock     : 66000000Hz
ipg per clock : 66000000Hz
uart clock    : 80000000Hz
cspi clock    : 60000000Hz
ahb clock     : 132000000Hz
axi clock   : 264000000Hz
emi_slow clock: 132000000Hz
ddr clock     : 528000000Hz
usdhc1 clock  : 198000000Hz
usdhc2 clock  : 198000000Hz
usdhc3 clock  : 198000000Hz
usdhc4 clock  : 198000000Hz
nfc clock     : 24000000Hz
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]
Boot Device: SD
I2C:   ready
DRAM:   1 GB
MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3
*** Warning - bad CRC or MMC, using default environment

In:    serial
Out:   serial
Err:   serial
Found PFUZE100! deviceid=10,revid=11
Net:   got MAC address from IIM: 00:04:9f:02:e4:78
FEC0 [PRIME]
Hit any key to stop autoboot:  3     2     1     0
PHY indentify @ 0x1 = 0x004dd074
FEC: Link is down 7949
Using FEC0 device
TFTP from server 192.168.1.101; our IP address is 192.168.1.103
Filename 'uImage'.
Load address: 0x10800000
Loading: * FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
FEC: Link is down 7949
T FEC: Link is down 7949
FEC: Link is down 7949"

 

Did anybody see this problem before?! How can it be fixed?

Appreciate your help. See also attachments.

 

Best, Ioan

Original Attachment has been moved to: cfg.ini.zip

Original Attachment has been moved to: ucl2.xml.zip

Original Attachment has been moved to: UICfg.ini.zip

Outcomes