Here is what is listed.
Full set of endpoints EP0-EP15 is only available when operating as a Device. The number of endpoints available is limited when operating as Host or OTG.
Isochronous Transfer - Available only in Full and High Speed modes with a maxium payload size of 1024 Bytes.
Interrupt Transfer - 8 bytes for Low speed, 64 bytes for Full speed, 1024 bytes for High speed.
Bulk Transfer - Full speed supports packet sizes of 8,16,32, or 64 bytes. High speed supports a packet size of up to 512 bytes.
Not sure if this the info you need.
Title of book is "Coldfire Microprocessors & Microcontrollers"
ISBN 0-9762973-0-2 AMT Publishing and was written by Freescale Engineers form what I can tell.