Hello friends,
I am new to Freescale and MQX RTOS developments.
I am using following environments,
Development board - FRDM-K22F120M
GT 202 MQX PDK,
SDK v1.2
IAR v7.20
Till now I have successfully compiled/built throughput_demo (sample application) as per GT-202_MQX_PDK_QSR.pdf.
My queries are,
1. Does MQX supports dynamic task creation like FreeRTOS supports?
2. How to know MQX RTOS type whether lite or something else ?
Hi
1. Yes, in MQX, any task can create another task by calling _task_create(), _task_create_at() or _task_create_blocked. and passing the processor number, a task template index, and a task-creation index, it is very similar to xTaskCreate() in FreeRTOS
2. In KSDK1.2, in file mqx_sdk_config.h, there is a macro, MQX_COMMON_CONFIG, it can set to MQX_LITE_CONFIG. -for lower memory usage, less features
Best regards
Daniel