AnsweredAssumed Answered

i.MX6 Solo Lite Compatibility with i.MX Dual Lite

Question asked by Mark Greenhalgh on Jul 30, 2015
Latest reply on Jul 30, 2015 by igorpadykov

I am using a few reference designs to help as I design and layout our board. One of the designs I am using has an i.MX6  SoloLite processor and most pins have been the same as those in the DualLite processor. I did notice some differences when I started into a part of our design using I2C. In the SoloLite design I am referencing, I2C2_SDA is pin D18 and I2C2_SCL is pin E18. In the DualLite, it appears that I2C2_SDA is pin C25 and I2C2_SCL is pin E22.

 

So, my questions are:

  1. Is the i.MX6 SoloLite pin compatible with the i.MX6 DualLite?
  2. Is there a better datasheet you can send me? (I am currently using the document: “i.MX 6Solo/6DualLite Applications Processors for Consumer Products”)
  3. Do you know of any reference designs that are available for the i.MX6 DualLite? (I can only find the Quad and SoloLite SabreSD reference designs)

Outcomes