For an example project in Freescale_MQX_4_2, "mfs_nandflash_twrk60f120m", I need to create ".hex" as a output in order to load into my device and check the functionality, I tried by changing the settings but even then it is throwing error. Could any help me to get rid from this issue? Reply me soon.
Hello Manigandan,
Open the project setting using the menu Project > Properties and go to C/C++ Build > Settings > Additional Tools and enable’Create Flash Image‘:
Now you need to press the Apply button:
Pressing the Apply button will show up an additional ‘Create Flash Image’ group.
Now you can specify hex as output format:
Pressing OK, and building your project again, you will show up the hex file together with the application file:
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------