Hello everybody.
I'm having problems with Input Capture at alternative pin at MC9S08PA32.
I am unable to count pulses at PTD1 pin. I think that there is a wrong in configuration code.
My assembly configuration code is:
LDA #%01011100
STA SYS_SOPT1
LDA FTM2_MODE
ORA #mFTM2_MODE_WPDIS
STA FTM2_MODE
LDA #%01000100
STA FTM2_C3SC
Does anybody know what is the problem?
Hi Fernando
Please check the attached project this is a CW 10.6 project for the tower PT60 that set the FTM2 CH3 on the PTD1 as input capture and also set the FTM1 as PWM, I use it to test the FTM2, unfortunately I am not good with assembly code, you can use the disassemble option on code warrior.
I hope this will help you.
Have a great day,
Vicente
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------