T4240RDB hung with sdk1.8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4240RDB hung with sdk1.8

605 Views
manojchaudhary
Contributor I

Hi All,

 

I was using SDK1.6 for my testing on T4240RDB board, but now i want to continue testing with SDK1.8. So for that i took SDK1.8 iso(QorIQ-SDK-V1.8-20150619-yocto.iso) and extracted it, after build i have loaded all images to nor flash. but i am facing issue with kernel booting, when u-boot is up it goes to kernel boot and there T4240RDB got hung after doing some CRC check with device tree file.booting logs are attached below-

Now with SDK1.6 working images also i am facing same issue.

May be i am doing some silly mistake, Please provide me some suggestion for resolving this issue.

 

Some logs are given below-

=====================================

## Booting kernel from Legacy Image at ec020000 ...

   Image Name:   Linux-3.12.37-rt51-QorIQ-SDK-V1.

   Image Type:   PowerPC Linux Kernel Image (gzip compressed)

   Data Size:    4804368 Bytes = 4.6 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at ed300000 ...

   Image Name:   fsl-image-core-t4240rdb-20150727

   Image Type:   PowerPC Linux RAMDisk Image (gzip compressed)

   Data Size:    39726545 Bytes = 37.9 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at ec800000

   Booting using the fdt blob at 0xec800000

   Uncompressing Kernel Image ... OK

   Loading Ramdisk to 2da1d000, end 2ffffdd1 ... OK

   Loading Device Tree to 03fde000, end 03fffc40 ... OK

=======================================

After booting up to here T4240RDB got hung.

 

Thanks,

Manoj

Original Attachment has been moved to: T4240RDB_hung_with_sdk1.8.txt.zip

Labels (1)
0 Kudos
1 Reply

323 Views
Pavel
NXP Employee
NXP Employee

The latest SDK for the T4240RDB board is SDK 2.0:

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...

 

Test your boar using u-boot and Linux kernel from this SDK.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos