In my custom i.mx6 board design, i m going to use LVDS and SATA which effects the current calculation of VDD_HIGH_IN as stated below. So base max current drawn is 125 mA as stated in datasheet, however i couldnt find any information regarding maximum current drawn from NVCC_LVDS_2P5 and SATA. There is typical current drawn from sata but not max. So how much current capability shall i allocate for VDD_HIGH_IN?
The note from the datasheet says:
"The actual maximum current drawn from VDD_HIGH_IN will be as shown plus any additional current drawn from the VDD_HIGH_CAP outputs, depending upon actual application configuration (for example, NVCC_LVDS_2P5, NVCC_MIPI, or HDMI, PCIe, and SATA VPH supplies)."
Solved! Go to Solution.
Hi Mehmet
VDD_HIGH_IN requirements are described in Sabre schematic spf-27392 p.20
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Mehmet
VDD_HIGH_IN requirements are described in Sabre schematic spf-27392 p.20
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you..