AnsweredAssumed Answered

MX280 nand flash MfgTool Download error

Question asked by PARK Sae Won on Jul 28, 2015
Latest reply on Jul 29, 2015 by igorpadykov

Dear All

 

Development Boards

nand flash MfgTool Download error

 

We board config

1. MX280

2. NAND Flash 1Gb (K9F1G08U0D - Samsung)

3. DDR2 1Gb

 

mfgtool.log

Tuesday, July 28, 2015 17:50:43

1 - Panel A Start processing Singlechip NAND <LIST/>. Panel A Start <CMD/> type="boot" body="Recovery" file="updater.sb" timeout="10" onError="" text="Booting Update Firmware.".

1 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater.sb" timeout="10" onError="" text="Booting Update Firmware." SUCCESS code=0x0. Panel A Start <CMD/> type="find" body="Updater" file="" timeout="180" onError="" text="". Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE Panel A UtpUpdate Event: DeviceArrival Msg: (null) DevState: Recovery OpState: WAITING_FOR_DEVICE

1 - Panel A Finished <CMD/> type="find" body="Updater" file="" timeout="180" onError="" text="" FAIL code=0xffff0002. Panel A: Wrong device found.,failed to run command: type="find" body="Updater" file="" timeout="180" onError="" text="" 

2 - Panel A Finished processing Singlechip NAND <LIST/> : FAIL code=-65534. Panel A: Reason is unknown,

 

What should I check?

 

Regards,

S.W. Park

Outcomes