AnsweredAssumed Answered

KSDK configuring MQX for Flexbus

Question asked by Matthew James on Jul 28, 2015
Latest reply on Aug 3, 2015 by Carlos_Musich

Hi

I'm using KDS studio 3 using KDSK 1.2 .

 

I've used Processor Expert to configure a KInetis K63 project, which has been a lot of trial and effort due to lack of documentation. - irrelevant.

 

I'm using MQX in round robin mode,( which doesn't seem to be supported in PE) -  irrelevant.

 

At the moment I'm trying to get the FLEXBUS to work to access RAM and an LCD

 

I've configured it in PE, Address and data lines, CS, OE, RW and set up 2 memory regions for the RAM and LCD.

 

I compile PE to generate the code and it  compiles and calls the FLEXBUS_DRV_Init routine.

 

Memory is currently set to be high at $A0000000

 

I'm confused as to whether I need to modify MQX to run with the Flexbus?

There are lots of outdated? notes on how to configure MQX for flexbus but these seem to refer to the original MQX not the MQX supplied with KSDK.

 

Is there a note on how to set up flexbus using PE with MQX?

Outcomes