JTAG J17 terminal connection.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JTAG J17 terminal connection.

Jump to solution
758 Views
takashitakahash
Contributor III

Hi community.

IMX6 SABRE AI CPU Card, at the Revision B, when  look at the circuit around JTAG CONNECTR of J17, JTAG_nTRST has not been connected to the J17.

(TRSTB terminal of iMX6 has H level is always input)

TRSTB terminal is the H level fixed, there is no problem?

Labels (2)
0 Kudos
1 Solution
623 Views
Yuri
NXP Employee
NXP Employee

   According to Table 2-19 (JTAG interface summary) of “Hardware Development
Guide for i.MX 6 …” :
JTAG_TRSTB input of i.MX6 has internal 47 kOhm pull up and

external pull up is not required; nevertheless it is possible to

apply external 10 kOhm pull up.

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
623 Views
sinanakman
Senior Contributor III

Hi Takahashi

In addition to Yuri's explanations please also

note that JTAG_nTRST is an optional pin

for JTAG debugging and most JTAG debuggers

can work without this pin (and reset the TAP

with a different sequence).

Hope this helps

Regards

Sinan Akman

624 Views
Yuri
NXP Employee
NXP Employee

   According to Table 2-19 (JTAG interface summary) of “Hardware Development
Guide for i.MX 6 …” :
JTAG_TRSTB input of i.MX6 has internal 47 kOhm pull up and

external pull up is not required; nevertheless it is possible to

apply external 10 kOhm pull up.

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos