Hi community.
How many synthesis of one IPU can be out put number of frame plane and the upper limit pixsel size and frame rate FPS(Frame par second)?
One of IPU in a Plane capable of synthesizing the number, size, and frame rate
Use the divide within the maximum output of the DP 240Mp/s?
Use the 4 Plane for all 30 fps @ 1920 x 1080.
It would require approximately more than 400Mp/s over, but one IPU has 240Mp/s.
Is it cannot be synthesized?
In this case how many synthesize screen plane?
Hi Takashi
you are right, for 4 planes output rate will be less, for capabilities one can look at
presentation below p.58
A Deep Dive into Image Processing for i.MX 6 Series Applications Processors
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------