AnsweredAssumed Answered

checksum error while building image for imx6qsabresd

Question asked by chandra shekar on Jul 26, 2015

I am trying to build image for imx6qsabresd.

I am facing below check-sum error.

How to resolve this..plz help me..

 

WARNING: Checksum mismatch for local file /home/roche01/fsl-yocto-3.10.53-1.1.0/downloads/firmware-imx-3.14.28-1.0.0.bin

Cleaning and trying again.

WARNING: Renaming /home/roche01/fsl-yocto-3.10.53-1.1.0/downloads/firmware-imx-3.14.28-1.0.0.bin to /home/roche01/fsl-yocto-3.10.53-1.1.0/downloads/firmware-imx-3.14.28-1.0.0.bin_bad-checksum_557586da46c952463090fe52e2854021

WARNING: Checksum failure encountered with download of http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//firmware-imx-3.14.28-1.0.0.bin;fsl-eula=true - will attempt other sources if available

WARNING: Renaming /home/roche01/fsl-yocto-3.10.53-1.1.0/downloads/firmware-imx-3.14.28-1.0.0.bin to /home/roche01/fsl-yocto-3.10.53-1.1.0/downloads/firmware-imx-3.14.28-1.0.0.bin_bad-checksum_19e66ff7d5530a2adbc09afa3776daae

ERROR: Checksum failure fetching http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//firmware-imx-3.14.28-1.0.0.bin;fsl-eula=true

ERROR: Function failed: Fetcher failure for URL: 'http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//firmware-imx-3.14.28-1.0.0.bin;fsl-eula=true'. Checksum mismatch!

File: '/home/roche01/fsl-yocto-3.10.53-1.1.0/downloads/firmware-imx-3.14.28-1.0.0.bin' has md5 checksum 39a101debacb84b282455dda31073ef3 when 6e700f3d3a6482db08d5aabee7751630 was expected

File: '/home/roche01/fsl-yocto-3.10.53-1.1.0/downloads/firmware-imx-3.14.28-1.0.0.bin' has sha256 checksum 28bc652060669aa0d35ada582199eeda0217d4162c1fb6b7431e3b7f616a0fcc when 1f09acd4d605efc78a0672068a658cb16274811d2f444cf3ae7aaa075266746f was expected

If this change is expected (e.g. you have upgraded to a new version without updating the checksums) then you can use these lines within the recipe:

SRC_URI[md5sum] = "39a101debacb84b282455dda31073ef3"

SRC_URI[sha256sum] = "28bc652060669aa0d35ada582199eeda0217d4162c1fb6b7431e3b7f616a0fcc"

Otherwise you should retry the download and/or check with upstream to determine if the file has become corrupted or otherwise unexpectedly modified.

 

 

ERROR: Logfile of failure stored in: /home/roche01/fsl-yocto-3.10.53-1.1.0/build_dir/tmp/work/cortexa9hf-vfp-neon-mx6qdl-poky-linux-gnueabi/firmware-imx/1_3.14.28-1.0.0-r0/temp/log.do_fetch.12532

ERROR: Task 1150 (/home/roche01/fsl-yocto-3.10.53-1.1.0/sources/meta-fsl-arm/recipes-bsp/firmware-imx/firmware-imx_3.14.28-1.0.0.bb, do_fetch) failed with exit code '1'

 

 

Regards

Chandra

Outcomes