I have just finished my first projects using the Freescale S12 MCU. I would like to thank everyone that help me.
In the past I have being using the Atmel AVR. The change to the Freescale was made easier with your help.
If there is one area were the AVR is a lot easier to work with, this is EEPROM. To me someone tried very hard to make it difficulty in the Freescale. Other then that I am very happy with the Freescale.
Here are pictures of the two projects.
http://www.turbofast.com.au/tfbin/CAN_EGT-8_PCB.jpg Eight channel EGT Amplifer using the S12G128
http://www.turbofast.com.au/tfbin/CAN_InterfacePCB.jpg CAN bus interface using the S12XE
Ray.