9s12HA48的问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

9s12HA48的问题

Jump to solution
1,727 Views
zcjxjw
Contributor I

我用BDM硬件 CodeWarrior5.1软件中的hiwave.exe读汽车仪表9s12HA48,0xBFF

读0xD8000-0xFBFFF时,只能读出0xD8000-0xDBFF 剩下的没读出来

软件的错误提示也不对:

Error: while reading memory from DC000

Reason: memory not defined in given range

 

但我从0xDC000-0xFBFF读也还是上面的提示 实际上从0xDC000根本没有 说明这个软件不能很好的区分cpu的flash

 

我估计读9s12的软件应该还有一个软件补丁 否则不能很好的读出数据

 

请高手 或厂家高手解决下难题

 

 

我还发现一个问题 实际只要把0x4000-0xFFFF读出来就可以了 因为一擦0x4000 0xD8000也跟着被擦掉了 把0x4000写上0xD8000也跟着写上了

我估计还是软件没有做到最好

但有的cpu跟着擦掉数据后 会丢失数据 还要再写一下  所以说BDM读9s12就是一头雾水 没有民间的设备好用 安全可靠

 

谢!

 

 

分还是要给你 你的方法还是麻烦 但我受到启发 搞定  官方的这个还是不太好用

Original Attachment has been moved to: f3.s19.zip

Labels (1)
0 Kudos
1 Solution
1,362 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi

please make sure all the memory you prepared to save is valid.

see my attached video.

Have a great day,

Zhang Jun
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
1,363 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hi

please make sure all the memory you prepared to save is valid.

see my attached video.

Have a great day,

Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos