AnsweredAssumed Answered

missing fsl-image-rds-ls1021aiot.ext2.gz.u-boot 

Question asked by Josh Smith on Jul 23, 2015

I am attempting to boot the ls1021aiot with linux following: http://cache.freescale.com/files/soft_dev_tools/doc/support_info/LS1021A-SDK-V1.1-ARM-SOURCE_RMF.txt .

 

 

I have tried recompiling several times, with 2 different packages, (rds, and full) but there is no fsl-image-rds-ls1021aiot.ext2.gz.u-boot or fsl-image-full-ls1021aiot.ext2.gz.u-boot file in the directory following compilation. Is the file hidden somewhere, or should it be included? The files that are included are:

 

 

fsl-image-full-ls1021aiot.manifest

fsl-image-full-ls1021aiot.tar.gz

fsl-image-full-ls1021aiot-20150723130459.rootfs.manifest

fsl-image-full-ls1021aiot-20150723130459.rootfs.tar.gz

iram_Type_A_LS1021a_r1.0.bin

modules--3.12-r0-ls1021aiot-20150721154641.tgz

modules-ls1021aiot.tgz

README_-_DO_NOT_DELETE_FILES_IN_THIS_DIRECTORY.txt

u-boot.bin

u-boot-ls1021aiot.bin

u-boot-ls1021aiot-2014.07-r0.bin

uImage    

uImage--3.12-r0-ls1021a-iot-20150721154641.dtb

uImage--3.12-r0-ls1021aiot-20150721154641.bin

uImage-ls1021aiot.bin

uImage-ls1021a-iot.dtb

folder: rcw

 

a screenshot of these folders is attached

 

Thanks!

Attachments

Outcomes