I am using imx6qsabresd board running fsl-image-multimedia-full linux 3.14.28 based image.
I want to access my board file system remotely over ethernet/usb.
So tell me the procedure how to access? or which packages i need to add in image?
And another i am using eclipse for cross compiling application for the board. I want to debug my application on my board from eclipse on my PC.
I configured ssh and gdb as per the yocto manual. But i think there are some package missing in my linux image.
So what's the procedure to enable this?
Hello,
Add this to your conf/local.conf
EXTRA_IMAGE_FEATURES = "debug-tweaks tools-debug eclipse-debug ssh-server-openssh"
CORE_IMAGE_EXTRA_INSTALL += "openssh-sftp openssh-sftp-server"
Regards,
Luis
You can configure ftp server on the board and access the filesystem from the outside of the board via ftp.
And you can use gdbserver for remote debugging the applications.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
i have configure ssh server. and able to access file system using sftp://root@ip_address:28.
But how to create ftp server?
i followed the below link to debug hello world application from eclipse.
http://developer.toradex.com/knowledge-base/hello-world-application-on-embedded-linux
Eclipse generate .o file. But how to generate .ko using eclipse?