AnsweredAssumed Answered

OMXPlayer start fail

Question asked by jack lu on Jul 22, 2015

Hi expert,

 

Please help to check the dumplog as attached file。

 

My analyse:

it seems happened when do pause->resume->pause->resume ->.....-

>pause->next song

The correct flow:

OMXPlayer( 2464): Pause player.

OMXPlayer( 2464): Stop Player.

OMXPlayer( 2464): start player.

 

the wrong flow in this case:

OMXPlayer: Pause player.

OMXPlayer: start player.

OMXPlayer: Start player timeout.

OMXPlayer: Stop Player.

 

Could you help to check it?

why it shows as below:

06-26 00:55:43.955  2468  4518 I OMXPlayer: OMX.Freescale.std.audio_render.android.sw-based wait command[0:3] timeout.

06-26 00:55:45.195  2468  2817 W audio_hw_primary: do_out_standby... 1085196496

06-26 00:55:45.365  3084  3084 D wpa_supplicant: RX ctrl_iface - hexdump(len=11): 53 49 47 4e 41 4c 5f 50 4f 4c 4c

06-26 00:55:45.365  3084  3084 D wpa_supplicant: wlan0: Control interface command 'SIGNAL_POLL'

06-26 00:55:45.385  3084  3084 D wpa_supplicant: nl80211: survey data missing!

06-26 00:55:48.385  3084  3084 D wpa_supplicant: RX ctrl_iface - hexdump(len=11): 53 49 47 4e 41 4c 5f 50 4f 4c 4c

06-26 00:55:48.385  3084  3084 D wpa_supplicant: wlan0: Control interface command 'SIGNAL_POLL'

06-26 00:55:48.405  3084  3084 D wpa_supplicant: nl80211: survey data missing!

06-26 00:55:49.435  2468  4518 I OMXPlayer: LEVEL: 1 FUNCTION: Start LINE: 804

06-26 00:55:49.435  2468  4518 I OMXPlayer: Start player timeout.

06-26 00:55:49.435  4271  4281 W MediaPlayer: info/warning (2, 0)

06-26 00:55:49.465  2468  2872 I OMXPlayer: Stop Player.

06-26 00:55:49.495  4271  4271 I MediaPlayer: Info (2,0)

 

thanks!

 

BTW: our android version is android_jb4.2.2_1.1.0

 

BRs

Jack

Original Attachment has been moved to: dumpstate.zip

Outcomes