Does IMX283's Ethernet port support both MII and RMII interfaces?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does IMX283's Ethernet port support both MII and RMII interfaces?

656 Views
linjiepan
Contributor II

Does IMX283's Ethernet port support both MII and RMII interfaces?

It seams that IMX283's Ethernet port only supports RMII interfaces, not suit for MII interfaces.

In the I.MX28 series,  only IMX287 supports MII interfaces and two  Ethernet ports ?

Labels (1)
0 Kudos
5 Replies

508 Views
Yuri
NXP Employee
NXP Employee

  The i.MX28 supports both MII and RMII modes ; from software point of view,
it is enough to setup correctly RMII_MODE bit in HW_ENET_MAC_RCR register.

Please look at section 26.4.9 "ENET MAC Receive Control Register

(HW_ENET_MAC_RCR)" of the  i.MX28 Reference Manual.

Only the i.MX287 contains two ENET modules.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

508 Views
linjiepan
Contributor II

Yuri

      IMX283 only has the PIN: ENET0_TXD0, ENET0_TXD1, ENET0_TX_EN,,ENET0_RXD0, ENET0_RXD1, ENET0_RX_EN, as showed on the< IMX28CEC.PDF>.

If IMX283 can supports both MII modes, where is the PIN of ENET0_TXD2,ENET0_TXD3,ENET0_RXD2 and ENET0_RXD3?

0 Kudos

508 Views
Yuri
NXP Employee
NXP Employee

The i.MX283  does not support MII (just RMII).

Regards,

Yuri.

0 Kudos

508 Views
linjiepan
Contributor II

Yuri

     thanks for your reply. So, In the I.MX28 series,  only IMX287 supports MII interfaces and two  Ethernet ports ?

0 Kudos

508 Views
Yuri
NXP Employee
NXP Employee

> So, In the I.MX28 series,  only IMX287 supports MII interfaces and two  Ethernet ports ?

Correct.

Regards,

Yuri.

0 Kudos