AnsweredAssumed Answered

How offten I should redetermine the 10-parameter for correction of Hard and Soft-Iron effect?

Question asked by Suqian Jin on Jul 19, 2015

I plan to develop a device that will have a MAG3110 magnetometer installed to measure device's direction. I understand that readings of the magnetometer must be corrected to eliminate Hard and Soft-Iron effect by using 10 parameters, which was determined after a device was completed, using freescale's method to get precise results. My question is should the 10 parameters be re-determined every time of using the device or just need to determine it only once, then store it in the device's memory, and reuse it forever? Thank you very much for your help. 

Outcomes