Hi,
I am facing a problem with video output from IMX6q sabrelite board.
I am feeding a video input through CSI0 of IPU0 as per the image attached below
But the output is as below from the HDMI interface
can anyone please suggest me whats wrong with the configuration or what might be the issue.
Thanks in advance.
Hi Sharath
for sabrelite board one needs to use BSPs built for that board, please look at
http://boundarydevices.com/tag/camera/
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov
I am using L3.0.35_4.1.0_ER_SOURCE_BSP
with linux 10.04 LTS which is, i think the board support package for imx6 sabrelite board.
This BSP is written and tested for freescale reference boards,
not sure that it supports sabrelite, though you can find sources there.
To be sure I would suggest to post that on
meta-fsl-arm mailing list, so maintainers for this board
could try to assist you
https://lists.yoctoproject.org/listinfo/meta-freescale
Best regards
igor