AnsweredAssumed Answered

iMX6 on-die temperature measurement

Question asked by Jai Ganesh on Jul 17, 2015
Latest reply on Jul 17, 2015 by Biyong Sun

Hello there,

 

Regarding the thermal management in iMX6, I can see that the bootloader (u-boot) does not allow to boot when the on-die temperature is greater than 80C. The macros used in bootloader are:

 

#define TEMPERATURE_MIN-40
#define TEMPERATURE_HOT80
#define TEMPERATURE_MAX125

 

Are these values with respect to commercial iMX6 processors or industrial iMX6 processors?

 

Thanks,

Jai Ganesh

Outcomes