AnsweredAssumed Answered

imx6 sabre smart devices board unable to send a signal when uart2 tx  transport text for minicom

Question asked by chen sam on Jul 15, 2015
Latest reply on Jul 20, 2015 by chen sam

hi,all:

why imx6 sabre smart devices board unable to send a signal when uart2 tx  transport text for minicom?

 

cpu can not send uart2_tx signal  to other side (pc end),but uart5、4、1 can.

 

Other:

android after boot uart3_tx can send signal  to drive GPS's tx (uart2_tx、uart3_tx set of 3.3V pin,uart1_tx、uart4_tx、uart5_tx set of 1.8V pin).

Might be power problems?

 

please help me,thanks.

 

(中譯:為何imx6 sabre smart devices board的uart2_tx不能由minicom 送出文字到另一邊(PC端),也就是cpu的uart2_tx信號完全無信號發出.

          但uart1、4、5卻是可以發出信號.

          其他:

          android 開機後,uart3_tx 卻能送信號去驅動GPS,不過是否是電壓問題呢?uart2_tx、uart3_tx 是設定在 3.3V pin,uart1_tx、uart4_tx、uart5_tx 是設定在1.8V pin)

)

Outcomes