AnsweredAssumed Answered

Examples / tutorials with PE but without KSDK?

Question asked by Rolf Freitag on Jul 15, 2015
Latest reply on Jul 22, 2015 by Rolf Freitag

I have to program a board with a MK60DNZVLL10, so i can make a project with PE but without KSDK.

I could do a basic configuration, timer configuration, via the CPU component, but there ist no component (i can add to the project and use) to configure the pins, e. g. the GPIO pins for LED toggling.

Is the only way to do it reverse programming, looking which functions are used in projects with KSDK, and do copy&paste them to main() or functions called by main()?

 

And where can i find examples / tutorials with PE but without KSDK?

Outcomes