We now use a board based on MCF54418,and its circuit is the same as development board(TWR-MCF5441x (700-26131))bought from freescale。
The Ethernet IC DP83849 use 50MHZ clk which is generate by the Oscillator serving for MCF54418.
And I want to use 2 Oscillator respectively,one for DP83849, and one for MCF54418. Is there any problem with my idea?
Hello Eric,
You need to make sure that the crystal is the same for both; MCU and PHY. If it is different then you will have asynchronous signals and this could be the problem.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------