AnsweredAssumed Answered

In the dual core VF6 can I only boot the m4 core to minimize system power in certain applications?

Question asked by Ken McDaniel on Jul 14, 2015
Latest reply on Aug 20, 2015 by alejandrolozano

Few questions on the VF6xx cores:


Can I only boot the m4 core (keeping the A5 off or stopped) in the VF6xx  to minimize system power in certain applications?

Will the m4 core have access to the nand and ddr controllers if the A5 core is off?

What are typical power measurement in low power modes if the m4 is running and the A5 core is off/stopped?

 

Thanks,

Ken

Outcomes