AnsweredAssumed Answered

Default security of TCP ports in MQX

Question asked by Akhil M V on Jul 14, 2015
Latest reply on Jul 16, 2015 by Carlos_Musich

Hi all,

Is there any default security in the RTCS network stack for the following situation? If yes, how to enable this?

 

     *     A TCP port (say 7564) is in opened state and the port is waiting for a valid connection.

     *     Then connections are tried from  the unknown sources continuously to that port. This causes the port busy state, which is unexpected.

 

Thanks

Akhil

Outcomes