Hi,
I am looking for reference document for how to configure MFG Tool for your custom board.
I want to do firmware update on eMMC.
- How to generate mfgtool firmware update images?
We are not able to start UTP Command.
Log is a as follows.
mmc1: no vqmmc regulator found
mmc1: no vmmc regulator found
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
mmc2: no vqmmc regulator found
mmc2: no vmmc regulator found
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mmc3: no vqmmc regulator found
mmc3: no vmmc regulator found
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_asrc 2034000.asrc: mxc_asrc registered
mxc_vpu 2040000.vpu: VPU initialized
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
mmc2: BKOPS_EN bit is not set
mmc2: new high speed DDR MMC card at address 0001
mmcblk2: mmc2:0001 S10008 7.12 GiB
mmcblk2boot0: mmc2:0001 S10008 partition 1 4.00 MiB
mmcblk2boot1: mmc2:0001 S10008 partition 2 4.00 MiB
mmcblk2rpmb: mmc2:0001 S10008 partition 3 4.00 MiB
mmcblk2: p1
mmcblk2boot1: unknown partition table
mmcblk2boot0: unknown partition table
wm8962 0-001a: Failed to read ID register
wm8962: probe of 0-001a failed with error -5
fsl-hdmi-dai hdmi_audio.17: failed to probe. Load HDMI-video first.
fsl-hdmi-dai: probe of hdmi_audio.17 failed with error -12
imx-wm8962 sound.28: failed to find codec platform device
imx-wm8962: probe of sound.28 failed with error -22
imx-audio-hdmi sound-hdmi.29: initialize HDMI-audio failed. load HDMI-video first!
TCP: cubic registered
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
VGEN3: disabling
VGEN2: disabling
SWBST: disabling
SW4: disabling
wm8962-supply: disabling
usb_otg_vbus: disabling
regulator-dummy: disabling
imx mcc test is registered.
g_serial gadget: Gadget Serial v2.4
g_serial gadget: g_serial ready
gpio-keys gpio-keys.27: Failed to request GPIO 6, error -16
gpio-keys: probe of gpio-keys.27 failed with error -16
snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
ALSA device list:
No soundcards found.
Freeing unused kernel memory: 328K (80bde000 - 80c30000)
Starting UTP
uuc 0.5 [built Jan 5 2015 14:47:13]
UTP: Waiting for device to appear
Hi Saurabh
I think one can look at presentation below, in particular p.59,71
describing custom configurations and mfg tools
https://community.freescale.com/docs/DOC-104266
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
igor
Thanks for reply.
I am using Android4.4.3.
Can we use kernel_imx\arch\arm\configs\imx_v7_mfg_defconfig to build kernel for MFG Tool?
it doesn't build.
What is a root cause for communication stop working after UTP?