Ethernet failure issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet failure issue

595 Views
vineethhegde
Contributor II

I am testing a board based on i.MX6Q processor. in that ethernet ping test is failed. The component mounting is done as per the  schematics. And every voltage , clock frequency are proper. Please suggest the solution.

Labels (1)
0 Kudos
3 Replies

429 Views
igorpadykov
NXP Employee
NXP Employee

Hi vineeth113

first check 125MHz clock, it should be outputed from ethernet phy and should have

correct duty cycle, if not, then you have to use a 125MHz oscillator for both i.MX6

and phy, the tolerance is +/-50ppm. Please check timings described in sect.4.11.5.3

RGMII Signal Switching Specifications IMX6DQCEC with oscilloscope

ENET_REF_CLK (ball V22) duty-cycle requirements on i.MX6

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

429 Views
vineethhegde
Contributor II

in that same board Ethernet phy IC is replaced then also issue persist.

0 Kudos

429 Views
igorpadykov
NXP Employee
NXP Employee

measure Ethernet phy timings using oscilloscope and

check with datasheet requirements

0 Kudos