Hi there,
I'm using a MCP5605B in Codewarrior 10.4 and I want to know how much RAM/ROM I'm using. I was able to do that with S12/S08 by looking at the .map file like this one:
/---------------------------------------------------------
Summary of section sizes per section type:
READ_ONLY (R): 8985 (dec: 35205)
READ_WRITE (R/W): 961 (dec: 2401)
NO_INIT (N/I): 12C (dec: 300)
/---------------------------------------------------------
Is there a way to have those informations with the MPC56? I don't want to manually sum all the object size in the .map
Thanks
I got the reply from our developers as below:
Unfortunately, the PA map file doesn’t print a nice summary of segment sizes for the users like some the other CW targets.
That said, the ELF file generated by PA is consumable by standard Linux/Cygwin tools such as ‘size’ and ‘readelf’. I suggest these as a quick solution.
test1> size *.elf
text data bss dec hex filename
19896 1780 832 22508 57ec test1.elf
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
Sorry for the Qorivva linker does not support the feature to display the total ROM/RAM size used in application project.
I have contacted the developers for this feature request and will update this post for any news.
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------