K60 interface with a parallel nor flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 interface with a parallel nor flash

953 Views
javiervicandi
Contributor II

Hello,

We need to use a parallel NOR flash memory with the K60. We have not found a memory with multiplexed address and data (size of 512Mb or 1Gb) to connect directly to FlexBus.

A solution without external latches or changing to serial interface?

Thanks

Labels (1)
2 Replies

771 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

K60 Flexbus module provides non-multiplexed address and data busses connection, which based on customer K60 pin resource.

If K60 could not provides enough non-multiplexed address pin resource, it need to use the address latches.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

771 Views
javiervicandi
Contributor II

Hi,

This is our case. We have pins only for multiplexed mode. We know some flash memory as the MT28GU01GAAA2EGC0SIT with A/D MUX but it needs 1.7V-2V supply.

We will check if it is possible reduce the VDD from 3.3V to 2V.

Best Regards

0 Kudos