Dear all,
upgrading from kernel 3.10 to 3.14 on imx6q sabre-auto similar board, i have a new warning, "use special clk parent"
mxc_sdc_fb fb.24: 1024x768 h_sync,r,l: 60,40,220 v_sync,l,u: 10,7,21 pixclock=65002000 Hz
imx-ipuv3 2400000.ipu: use special clk parent
imx-ipuv3 2400000.ipu: disp=1, pixel_clk=65002000 75428571 parent=75428571 div=1
Is this warning meaning i am doing something wrong in dts side, or i can ignore it ?
Best regards
Angelo Dureghello
Hi Alejandro,
thanks,
For what i understand from the code, is a new warning generated when parent ipu node "ldb_xx" clocks are used. Looking other boards dts, getting clock from parent should be fine.
Hi,
As I see, it is not a waning nor an error.
The message shows that the clock parent for the IPU is the same as the LBD_DIx_IPU
/Alejandro