AnsweredAssumed Answered

how to get uboot shell (U - Boot>)

Question asked by srinivasaporam on Jul 3, 2015
Latest reply on Aug 1, 2016 by Pranav Madhu

Hi,

We have got the I.MX6 reference board (Wandboard Quad). Serial port of this board is connected to Host PC which is running with Ubuntu and minicom. When we are powering the board, we are getting the messages. when it is asking for "Hit any key to stop autoboot" we are pressing spacebar/ESC. then it is stopping at =>. How to get the U-Boot shell (U-Boot>)

 

Please find the output of the minicom window as follows:

 

 

U-Boot 2014.04 (Jun 01 2014 - 21:28:55) armhf.com

 

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

Reset cause: POR

Board: Wandboard

DRAM:  2 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

*** Warning - bad CRC, using default environment

 

In:    serial

Out:   serial

Err:   serial

Net:   FEC [PRIME]                                                            

Hit any key to stop autoboot:  0

 

=>

Outcomes