Hi ,
I am using the Freescale micro Cobra 55 controller, MPC5777C , for my application.
1. Is there any way i can read the Checker Core running status from any registers instead of SIU_LOCKSTEP register where it shows only Lock step core is enabled or not? But if i wanted to know even though it is enabled , how to make sure that it is running or not?
2. If there is any failure in the Checker core, i need to check only FCCU status?
1) There is FCCU non-critical fault 42 indicating checker core is disabled.
2) Yes, faults 10 and 11.