LPDDR2 frequency change in imx6solo ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPDDR2 frequency change in imx6solo ?

573 Views
ela_embedded
Contributor I

we are using micron LPDDR2  interfaced with imx6solo in our customized board . DDR has three modes of speed grade with 533MHZ , 400 MHZ and 333 MHZ  . we need to configure our mmdc to 333MHz  for power optimization . Is this possible ? i have  gone through the reference manual but i didnt found the required information for mmdc.

Labels (1)
Tags (2)
0 Kudos
1 Reply

489 Views
igorpadykov
NXP Employee
NXP Employee

Hi ela

yes this is possible, for procedure one can look at attached document

Chapter 21 Dynamic Bus Frequency Driver from L3.14.28_1.0.0_iMX6QDLS_BUNDLE

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos