Dear community,
We hope to know the DDR_SEL setting of the IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE register.
We know that the register should be set according to description in RM:
10 : LPDDR2
11 : DDR3
[Question]
When we use the DDR3L ,
Which setting should we use ,"10" or "00"
on IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE : DDR_SEL ?
Best Regards,
Koichi Sakagami
Solved! Go to Solution.
Please use DDR_SEL = DDR3.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Please use DDR_SEL = DDR3.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------