In our IMX6 design we will use MMPF0100F3 (OTP)
I have two questions:
1) What about non used LDO ? I don't need all 6 LDO.
My space is critic and I want to eliminate as more as possible components
(for example CAP in and CAP out).
For example I need only VGEN4 , Can I simple not mount input and output CAP
for all other LDO.
2) for MMPF0100F3ANES in preprogrammed OTP configuration for some LDO
(VGEN2,VGEN3,VGEN6) in field "default voltage" we gave sign "-".
Does it mean that default these LDO are disabled ?
Thank in advance
1) For the information on the MMPF0100 unused pins connection, please refer to the Table 1 of the AN4717 Rev.3.0 App Note document, available on the MMPF0100 Documentation web page:
2) The "-" status of the MMPF0100 power supplies in the "Start-up configuration" table of the MMPF0100 Data Sheet document means that these supplies are not turned on during initial start-up. They can be turned on in software later.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------