Ethernet Audio Video Bridging support in i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet Audio Video Bridging support in i.MX6

1,978 Views
ko-hey
Senior Contributor II

Hi all,

I have question about Ethernet AVB.

In my understanding, Ethernet AVB needs to confirm to the following standard.

• 802.1BA-2011 AVB (Audio Video Bridging)

• 802.1AS-2011 gPTP (Generalized Time Precision Protocol)

• 802.1Qat-2010 SRP (Stream Reservation Protocol)

• 802.1Qav-2009 FQTSS (Forwarding and Queuing of Time Sensitive Streams)

• 1722-2011 AVTP + MAAP (Audio Video Transport Protocol, MAC Address Acquisition Protocol)

• 1722.1-2013 AVDECC (Audio Video Discovery, Enumeration, Connection Management and Control)

• 1722a D13 AVTP

1. Does i.MX 6SoloX support above standard in hardware ?

2. Does i.MX 6 series except SoloX not support in hardware?

3. if user want to use AVB in i.MX6 except SoloX, user have to use "Audio Video Bridging Software|Freescale​" .

    Is it correct ?

ko-hey

Labels (1)
Tags (2)
0 Kudos
3 Replies

875 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello ko-hey,

I would recommend looking at the AVB software specifications (link below) which mentions the standards implemented.

http://cache.freescale.com/files/soft_dev_tools/doc/fact_sheet/AVBRIDGSFWFS.pdf

The i.MX6SX does support AVB in Hardware, as mentioned on the i.MX6SX Datasheet, although the individual standards are not specified in detail.

Only the i.MX6SX supports AVB in Hardware in the i.MX6 Series family.

The AVB Software is required in order to have AVB implemented on any of the i.MX6 processors. The difference is that the i.MX6SX does support to run this standard in Hardware and the rest of the i.MX6 requires a Software implementation of the standard.

0 Kudos

875 Views
jianhuawang
Contributor I

gusarambula

What is the difference of the AVB implementation in hardware and software?

0 Kudos

875 Views
ko-hey
Senior Contributor II

Hi gusarambula

Sorry for late reply.

I understood.

Thanks!

ko-hey

0 Kudos