HI,
1:Can the MIPI CSI-2 interface of IMX6Q support 4-ch 1280*720p60 or 30 camera video input at the same time? it has 4 lanes CSI-2.
2:is there a method for 4-ch HD(1080*720P60 or P30) camera video input on IMX6Q? what is the interface?CSI-2 or PCIE?
HI 翔 李
IPU CSI-2 performance 400MB/s is given below
PCIe performance 100-200MB/s
i.MX6Q PCIe EP/RC Validation System
1. so seems 4-ch 1280*720p30 can be achieved (assuming YUV422 = 2 byte/pixel) with CSI-2
2. probably one can try 2 ch connect to PCIe, another 2 - to CSI-2
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------