AnsweredAssumed Answered

Using VOUT33 as main power for a K60

Question asked by Jean-Paul Deryck on Jun 25, 2015
Latest reply on Nov 18, 2015 by Mike Stroven

Hello,

I would like to know if we can always use the VOUT33 (with VREGIN connected to a 5V source and internal regulator enabled) as the main source of power for the K60 ?

I see that output current of VOUT33 is maximum 120 mA, is there a case when it is not sufficient for the K60, for example when all peripherals are enabled ?

best regards

JP

Outcomes