Hi,
I'm currently working with MX6Q and Ltib L3.0.35_4.1.0.
The gstreamer included in L3.0.35_4.1.0 is 0.1x and I would like to switch to gstreamer-1.x.
Seems that fsl-L3.14.28_1.0.0_iMX6qdls_Bundle comes with gstreamer-1.x.
But I do not want to change my kernel and drivers.
So is there a way to use gstreamer-1.x and the corresponding FSL video plugins with linux kernel 3.0.35( from LTIB L3.0.35_4.1.0)?
Thanks,
Robbie
Hi Robbie
I am afraid this is not possible, since plugins are compiled for
specific kernel, as discussed below
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------