AnsweredAssumed Answered

xorg-server error using LTIB to build FSL gnome release system for i.MX6Q SabreSD board

Question asked by MeiHui Cao on Jun 24, 2015
Latest reply on Sep 20, 2015 by Peter Chiu

Hi,

 

I am using imx6q sabresd board.I am trying to build a linux system based on the BSP of L3.0.35_4.1.0_130816_source.tar.gz, and the OS of my host PC is Ubuntu 14.04. But when I built the FSL gnome release package system, I met an error as follows:

 

configure: error: tslib must be installed to build the tslib input driver.

error: Bad exit status from /home/b54871/i.MX6DQ_SDP/L3.0.35_4.1.0_130816_source/cmh/ltib/tmp/rpm-tmp.79842 (%build)

 

RPM build errors:

    Bad exit status from /home/b54871/i.MX6DQ_SDP/L3.0.35_4.1.0_130816_source/cmh/ltib/tmp/rpm-tmp.79842 (%build)

Build time for xorg-server: 15 seconds

 

Failed building xorg-server

 

f_buildrpms() returned an error, exiting

traceback:

main:572

 

Started: Wed Jun 24 15:35:22 2015

Ended:   Wed Jun 24 15:36:12 2015

Elapsed: 50 seconds

 

These packages failed to build:

xorg-server

 

Build Failed

 

Exiting on error or interrupt

 

 

Can anybody please help me with this issue?

Outcomes