AnsweredAssumed Answered

Using MMA8452Q For tilt alarm detection

Question asked by Jérôme MATHIEU on Jun 24, 2015
Latest reply on Jun 24, 2015 by Jose Alberto Reyes Morales

Hello ALL,

 

My project is to detect an angle of about +/- 40 ° relative to an initial position .

 

I am a newbie in accelerometer domain and the concepts covered in the data sheet are not very clear in my mind

 

I'll try to ask simple questions have simple answers

 

1°) Is it possible to do that with MMA8452Q ?

 

2°) Is there an application note that clearly explains the implementation of my project with the MMA8452Q ?

 

thank you very much

Sincerely

 

Jérôme.

Outcomes