Hello,
We are using the 'MOTUSB' driver for communication with MCF5272 processor. We are facing some problem in adding the code to the MOTUSB driver.
Problem Statement:
We want to send an integer data using the exsisting functions in motusb.lib, from the host to the device(MCF5272 processor). For this application, which function is best suitable and which parameter/s of the function can be used for this?
OR
Does anyone have the code for motusb.lib ?
Any suggestions on this implementation are welcome.
Regards
Ashwin.