I am building an application that requires a response to commands be sent through a UART. I am sending an 11 byte response string at 115200 baud, but it is taking twice as long to transmit than if it was send as one block.
I looked at the UART code, and it appears that the code is sending the data in the block one byte at a time.
Is there a way to pass the send the information in one packet so that we can get the transmission time to the proper period?
Solved! Go to Solution.
When nothing intervenes between the characters, then the transfer time is reasonably close.
However, the library I was using incorporates a EnterCritical() function just before the transmission of each character. That adds about 109 microseconds per character send; for 11 bytes that adds more than a millisecond to the transfer time. Once I put the EnterCritical and ExitCritical functions outside of the loop, that fixed the problem.
I figured I should make mention of what the solution finally turned out to be.
Hello Steven,
(1) Do you want a UART function that send numbers of bytes ?
If yes, which IDE do you use , if you use KDS, you can create e PE project , then utilize the function of
"LDD_TError AS1_SendBlock(LDD_TDeviceData *DeviceDataPtr, LDD_TData *BufferPtr, uint16_t Size)"
the "Size" is the number of bytes.
(2) "I looked at the UART code" , which code ?
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I just noticed that you are using the Serial_LDD code package. I derived my UART code from the AsynchroSerial package.
Is the SendBlock implementation going to be slower than the one derived from the Serial_LDD? If so, would it then behoove me to refactor my top level to use routines derived from Serial_LDD?
Hello Steven,
(1) "AS1_SendBlock" and the "AS1_SendBlock" are the same .
(2)Sorry i can not know your problem clearly. Could you pleas tell me how can i repeat your situation ? Especially repeat "resulting in a transfer time of 1.05ms instead of > 2ms?" thank !
About "have the effect of creating a delay between character writes" ,i have checked the code , there have not intended delay, the delay is the necessary configuration .
BR
Alice
(2)Sorry i can not know your problem clearly. Could you pleas tell me how can i repeat your situation ? Especially repeat "resulting in a transfer time of 1.05ms instead of > 2ms?" thank !
About "have the effect of creating a delay between character writes" ,i have checked the code , there have not intended delay, the delay is the necessary configuration .
Which code are you talking about? Are you using an interrupt-based (non-blocking) TX and RX setup with the Serial_LDD routines? I was using the AsynchroSerial library generated by Processor Expert.
Do you have sample code for the earlier, if you created it with Serial_LDD?
Instead of using the SendBlock function in the Serial_LDD component, I loaded the AsynchroSerial UART component and used the UART_SendBlock routine from that component.
They may be the same in the prototype level, but the later calls the former.
Here is a scope trace showing the issue.
The bottom trace (Channel 2) is the packet put out on the UART TX line. If the byte-to-byte spacing is the way it ought to be, it should take up a little more than one major division of the scope, or 1ms. It's taking up two milliseconds, or two divisions.
When you run a packet through SendBlock in Serial_LDD, what are you seeing?
When nothing intervenes between the characters, then the transfer time is reasonably close.
However, the library I was using incorporates a EnterCritical() function just before the transmission of each character. That adds about 109 microseconds per character send; for 11 bytes that adds more than a millisecond to the transfer time. Once I put the EnterCritical and ExitCritical functions outside of the loop, that fixed the problem.
I figured I should make mention of what the solution finally turned out to be.
Hello Steven,
The baud rate 115200 meaning UART can transmit 115200 bit every second .
And you can use the " time / bits " , the result is about 115200 .
Hope it helps
Alice
I am looking at the PE generated AsynchroSerial component for UART1. It has a UART_SendBlock method that I called, where the SerialLdd1_SendBlock function is called, and it is sending only one bit at a time.
Hello Steven,
As we know, the UART Data register only have 8 bits, so it sending only one byte at a time .
BR
Alice
Does that mean that, for the KEA64, the functions to send and receive block data are really only capable of passing one character at a time?
In which case, the ReceiveBlock can only capture one byte at a time, and can only take 1U as the length parameter? Is that the same for the SendBlock function as well?
It sounds to me like I've made the wrong point.
I understand that the routine will write to UART1 Data Register one byte at a time, but it's the transfer rate between writes that is the problem with the routine generated by PE in KDS.
It appears to have the effect of creating a delay between character writes such that the packet transfer time is twice as much as expected. Is there example code that uses AS1_SendBlock such that the inter-character spacing is more normal (resulting in a transfer time of 1.05ms instead of > 2ms?