Hello all,
I have a P&E multilink Universal programmer. I am using MC9s12c µP with 8MHz clock. What should be MCU speed in Flash page? I have always 1.41MHz even I have 8MHz clock. Is my clock dead or do I have to set some settings somewhere? Scope shows nice 8MHz.
Should I do anything else than set CLKSEL = 0x00; in SW?
This happened now with 4 different µP. Problem in Multilink firmware?
Hi,
You're using P&E Multilink Universal interface.
The last version is Rev C.
I don't know if this can help but a new firmware version has already solved problem with this interface under MCU V10.6 Update4 (Eclipse) and on CW for MCF V7.2 (Classic).
Please have a look to the post:
Problem with Multilink Rev C - not running after MCU V10.6 Update4 installed & CW for MCF V7.2
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------