I try to send out two 8bytes data in my firmware by using S12DP512. Once I set the CANXTFLG to 0x01, data would be sent on the CAN bus continuously. It is non stop.
Can anyone tell me what's happen to the bus? Below is my source code.
// *******************************************
if(CANXTFLG != 7) {
CANXTARQ = 0x7;
}
while(CANXTFLG != 7);
b_ptr = (unsigned char*)(&(cdata.c118));
CANXTBSEL = 0x01;
CANXTXIDR0 = ID118_0;
CANXTXIDR1 = ID118_1;
CANXTXIDR2 = ID118_2;
CANXTXIDR3 = ID118_3;
CANXTXDSR0 = *b_ptr++;
CANXTXDSR2 = *b_ptr++;
CANXTXDSR1 = *b_ptr++;
CANXTXDSR3 = *b_ptr++;
CANXTXDSR5 = *b_ptr++;
CANXTXDSR4 = *b_ptr++;
CANXTXDSR6 = *b_ptr++;
CANXTXDSR7 = *b_ptr++;
JEVS_CANXTXDLR = 8;
JEVS_CANXTXTBPR = 1;
JEVS_CANXTFLG = 0x01;
b_ptr = (unsigned char*)(&(cdata.c109));
JEVS_CANXTBSEL = 0x02;
JEVS_CANXTXIDR0 = ID119A_0;
JEVS_CANXTXIDR1 = ID119A_1;
JEVS_CANXTXIDR2 = ID119A_2;
JEVS_CANXTXIDR3 = ID119A_3;
CANXTXDSR0 = *b_ptr++;
CANXTXDSR2 = *b_ptr++;
CANXTXDSR1 = *b_ptr++;
CANXTXDSR3 = *b_ptr++;
CANXTXDSR4 = *b_ptr++;
CANXTXDSR5 = *b_ptr++;
CANXTXDSR6 = *b_ptr++;
CANXTXDSR7 = *b_ptr++;
CANXTXDLR = 8;
CANXTXTBPR = 2;
CANXTFLG = 0x02;
CANXTIER_TXEIE1 = 1;
Hi Mr. Wu,
There is at least another active CAN node on the same CAN BUS line ?
If no other node assert the acknoledgment bit, your device will continuosly re-send the very same frame .
Dear GottiLuca,
I am using something like CAN emulator on PC side. I am sending a CAN data
frame from S12DP512 to this emulator.
I set the emulator to listen mode only. Should I set the emulator to
normal mode?
I have another question about the buffer configuration. if I only use one
CAN bus for communication, Can I only have 3-levels priority setting
because I only have 3 transmitting buffer, right?