AnsweredAssumed Answered

Output compare mode setup using Flex timer module in KDS 1.2.0 ok to use?

Question asked by Chad Williams on Jun 22, 2015
Latest reply on Jun 29, 2015 by Jorge_Gonzalez

I have noticed in the reference manual for KDS1.2.0 page 559 it says:

The current Kinetis SDK driver only supports the generation of PWM signals. The input capture

and output compare will be supported in upcoming Kinetis SDK releases.

 

But in fsl_ftm_driver.c theres a function: FTM_DRV_SetupChnOutputCompare()

so that would indicate the functionality exists already. But there is no example code

to demonstrate output compare mode and Processor Expert doesn't allow me to

select Output Compare mode in the ftm driver component.

 

Output compare mode is necessary for driving motors etc so its an important feature

of many embedded microcontrollers.

 

Can anyone confirm FTM_DRV_SetupChnOutputCompare() does work ?

Outcomes